Liquid Level Sensors
Measure the liquids in tanks, containers, or other apparatus with the many level sensors available here at RS. We have options from leading brands that ensure accuracy and reliability when you use their devices.
There are many different types of liquid and water level sensors available including capacitive and ultrasonic, which can help with a range of different applications. So, browse the full range below to find the right one for you.
You can also make your search easier by using our advanced filters to create a personalized set of results to look through. This includes filters like manufacturer, type, output, supply voltage, and others.
Got a question? Get in touch with us today and we'll do our best to assist you.
Where can I find water level sensors?
The liquid levels we stock can be used in a whole range of industries to ensure accuracy is always on point. Here are a few examples:
- Food and beverage industry - to detect the consistency or smoothness of a product as well as ensuring the right amount of liquid appears in each bottle.
- Sewage treatment - to detect gas build-ups in waste or monitor potential clogging to make companies aware of areas that need cleaning.
- Sea level monitoring - can detect when sea levels are rising, which could indicate potential flooding as well as incoming tsunamis.
What kinds of water level sensors are available?
Pressure
This type of sensor can be found in water tanks or reservoirs and detects liquid levels through the amount of pressure being put on it. This is done through a tube in the sensor which can detect the amount of air in it to give a level value.
Ultrasonic
Ultrasonic water level sensors are a non-contact option suited to measuring things like oil and grease, but can also be used for solids such as sand and cement too. This sensor works by emitting ultrasonic waves and then measures how long it takes the reflected waves to go back to the sensor to give a fluid level value.
Capacitive
A capacitive liquid level sensor measures the change of capacitance and liquid unevenness. This is done by placing a metal rod in your water tank which creates a medium of gas and liquid between the rod and the tank walls. This medium will have a dielectric constant which will change when the liquid levels increase and decrease. Unevenness between these electrodes will indicate a change in liquid levels.
Radar
This sensor measures liquid levels by sending a high radio frequency from an antenna through an air gap. The amount reflected will determine the level height of the liquid you're measuring.
Float levels and switches
Water level float switches can measure the levels in tanks or larger bodies of water by placing them at the top of the liquid. These are commonly used in sewage pumps and liquid transfer pumps and consist of a reed switch and pivoted magnet. The switch is at the top of the liquid and any changes to its level result in the reed switch making adjustments, such as turning on or off the water pump.
What are the benefits of using water level sensors?
- Energy efficient - electricity usage is limited with this device, which allows more power to be saved.
- Automatic - once installed, these devices can be left to operate without the need for human interaction.
- Mostly non-contact - this means your water isn't at risk of contamination from too many parts touching it.
- Reliable - advancements in water level sensor development mean the life span and accuracy of these devices is prolonged.
- Easy installation - simple fitting means someone on your team may be able to install it, saving you money and time by not having to hire a professional to do it.
Why buy liquid level sensors from RS?
Over the years, we've built close relationships with leading manufacturers in the industry to ensure that we only supply the best products. You'll find the likes of B/W Controls, GEMS Sensors, Inc., and SICK in our water level sensors range, and these can offer durability and high levels of accuracy for your peace of mind.
We're one of the largest distributors of electrical goods in North America. We process and ship orders often on the same day from our technologically advanced distribution center in Texas. This means you won't have to wait long to start accurately measuring your liquid levels.
Make your shopping experience simple by narrowing your search with our advanced filtering options. If you need any extra help, then don't hesitate to get in touch and our trade experts will assist you. You can also find guides and industry updates in our expert hub to keep up to date with all things electronic.
On Order: 20
On Order: 21
On Order: 4
On Order: 20
On Order: 21